EEO#.PULSEWIDTH
Description
The pulse width of the pulses from the CW/CCW and step/dir modes,EEO#.MODE 1 or 2. In these modes this parameter also controls the width of the Z pulse. This parameter has no effect in the A quad B mode.
-
- If the pulse width is too long it will effect the maximum speed of the output as the pulses will start to overlap. This formula is expressed as:
MaxVelocity (rev/sec) <= 1/(Lines * PulseWidth_in_secs).
Examples
Code
This will set the pulse width to 8.16 us.
-->EEO1.PULSEWIDTH 8.16
Context
For more information see Output - Encoder Emulation.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read/Write |
Units | us |
Range | 0.08 to 2621.40 |
Default Value | 4.08 |
Data Type | Float |
See Also | |
Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
EEO1.PULSEWIDTH |
4600h |
04h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
EEO2.PULSEWIDTH |
4601h |
04h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
EEO3.PULSEWIDTH |
4603h |
04h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
EEO4.PULSEWIDTH |
4606h |
04h |
Unsigned32 |
- |
1000:1 |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
32015 |
1 |
32015 (0x7d0f) |
EEO1.PULSEWIDTH |
Signed32 |
Read/Write |
Yes |
32016 |
1 |
32016 (0x7d10) |
EEO2.PULSEWIDTH |
Signed32 |
Read/Write |
Yes |
32017 |
1 |
32017 (0x7d11) |
EEO3.PULSEWIDTH |
Signed32 |
Read/Write |
Yes |
32018 |
1 |
32018 (0x7d12) |
EEO4.PULSEWIDTH |
Signed32 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
EEO1.PULSEWIDTH |
32015 |
Float |
Read/Write |
- |
EEO2.PULSEWIDTH |
32016 |
Float |
Read/Write |
- |
EEO3.PULSEWIDTH |
32017 |
Float |
Read/Write |
- |
EEO4.PULSEWIDTH |
32018 |
Float |
Read/Write |
- |